RTD for s32k3 example project compilation error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RTD for s32k3 example project compilation error

Jump to solution
1,722 Views
JhonYF
Contributor III

 

Using the example under the RTD path, I directly imported it into S32DS for compilation, but an error occurred. How should I handle this?

PATH:SW32K3_RTD_R21-11_4.0.0_HF_02\eclipse\plugins\Adc_TS_T40D34M40I0R0\examples\S32DS

JhonYF_0-1753770748308.png

 

 

 

0 Kudos
Reply
1 Solution
1,713 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

If you want to test the RTD examples in S32DS, please click: File ->  New -> S32DS Project from Example -> S32K3XX AUTOSAR R21-11 RTD 4.0.0 HF02 D2407 Example Projects -> Adc Examples ->

Then follow the description.txt of the example:
3.1 Generating the S32 configuration
Before running the example a configuration needs to be generated. First go to Project Explorer View in S32 DS and select the current project. Select the "S32 Configuration Tool" menu then click on the desired configuration tool (Pins, Cocks, Peripherals etc...).
Clicking on any one of those will generate all the components. Make the desired changes (if any) then click on the "S32 Configuration Tool->Update Code" button.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

View solution in original post

0 Kudos
Reply
2 Replies
1,714 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

If you want to test the RTD examples in S32DS, please click: File ->  New -> S32DS Project from Example -> S32K3XX AUTOSAR R21-11 RTD 4.0.0 HF02 D2407 Example Projects -> Adc Examples ->

Then follow the description.txt of the example:
3.1 Generating the S32 configuration
Before running the example a configuration needs to be generated. First go to Project Explorer View in S32 DS and select the current project. Select the "S32 Configuration Tool" menu then click on the desired configuration tool (Pins, Cocks, Peripherals etc...).
Clicking on any one of those will generate all the components. Make the desired changes (if any) then click on the "S32 Configuration Tool->Update Code" button.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 Kudos
Reply
1,708 Views
JhonYF
Contributor III
Thank you very much for your reply
0 Kudos
Reply