RTD / ICU example for SK148 broken?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RTD / ICU example for SK148 broken?

ソリューションへジャンプ
1,593件の閲覧回数
billr
Contributor I

I've generally had no problems with the various RTD examples I've tried to run. However, the Icu_BlinkLed_ASR_Ftm_S32K148 example does not seem to work as expected. The LED does not blink and the ISR is never called. Has anyone run into this problem?

(This is related to my earlier question about a button example, in the sense that one post suggested using the ICU, but if the ICU example doesn't work, that's very helpful.)

0 件の賞賛
返信
1 解決策
1,566件の閲覧回数
DanNguyenDuy
NXP Employee
NXP Employee

Dear billr,

Please read this file and connect pins as requirement:

nxf78987_0-1653533598571.png

Best regards,

Dan

元の投稿で解決策を見る

1 返信
1,567件の閲覧回数
DanNguyenDuy
NXP Employee
NXP Employee

Dear billr,

Please read this file and connect pins as requirement:

nxf78987_0-1653533598571.png

Best regards,

Dan