RTD / ICU example for SK148 broken?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RTD / ICU example for SK148 broken?

Jump to solution
1,592 Views
billr
Contributor I

I've generally had no problems with the various RTD examples I've tried to run. However, the Icu_BlinkLed_ASR_Ftm_S32K148 example does not seem to work as expected. The LED does not blink and the ISR is never called. Has anyone run into this problem?

(This is related to my earlier question about a button example, in the sense that one post suggested using the ICU, but if the ICU example doesn't work, that's very helpful.)

0 Kudos
Reply
1 Solution
1,565 Views
DanNguyenDuy
NXP Employee
NXP Employee

Dear billr,

Please read this file and connect pins as requirement:

nxf78987_0-1653533598571.png

Best regards,

Dan

View solution in original post

1 Reply
1,566 Views
DanNguyenDuy
NXP Employee
NXP Employee

Dear billr,

Please read this file and connect pins as requirement:

nxf78987_0-1653533598571.png

Best regards,

Dan