RTD GPT configuration

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

RTD GPT configuration

跳至解决方案
254 次查看
durga_choudhury
Contributor III

The details of the HW/SW this question pertains to is this:

S32K148 (on a custom board)

S32 Design Studio for S32 Platform

Version: 3.6.2

Build id: 250529 (Update 2)

 

The RTD version is as shown below:

durga_choudhury_0-1758920952334.png

 

I am including a GPT to my project. I want it to count up from 0 to 5000 and start over. The problem I am facing is there seems to be no way to configure this upper bound. This is a 16 bit counter and the SDK configurator does not seem to like any value other than 65535 (trying to do so makes the project invalid, please see the screenshot below:

durga_choudhury_1-1758921184994.png

 

If this value can only take a fixed value (65535) then I don't see it being a configurable parameter (and useful)

If this can take any value from 1 up to 65535 then the tool seems to be broken.

 

The only workaround that I have found is to change

#define FTM_CNT_MAX_VALUE 0x0000FFFF

to

#define FTM_CNT_MAX_VALUE 5000

in Ftm_Gpt_Ip.h (knowing that any such change will be overwritten the next time code is regenerated, but that is my only way to make progress right now)

If I am mistaken, please correct me. If not, please advise on the best way to proceed.

标记 (2)
0 项奖励
回复
1 解答
147 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @durga_choudhury 

It is shown as configurable in the Peripherals view because the driver is designed to be flexible. It can be reused to configure other timers with different resolutions, so having that value exposed makes it easier to adapt the setup for different use cases.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
199 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @durga_choudhury 

I think there may be a misunderstanding regarding the GptChannelTickValueMax parameter. This value represents the maximum number of ticks that a channel can count. Since the FTM is a 16-bit timer, the resolution is:

2^{16} − 65,535 ticks

This value is mandatory, and that is why an error is displayed if a different value is set.

To define the desired timeout period for the channel, you should use the Gpt_StartTimer() function. For reference, you can consult the Gpt_example_S32K148 included with the RTDs.

 

BR, VaneB

0 项奖励
回复
194 次查看
durga_choudhury
Contributor III

Hello @VaneB 

 

Thanks for the clarification. I am still confused as to why a number that is a hard constant is configurable on the Peripherals view.

 

Regards

Durga Choudhury

标记 (2)
0 项奖励
回复
148 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @durga_choudhury 

It is shown as configurable in the Peripherals view because the driver is designed to be flexible. It can be reused to configure other timers with different resolutions, so having that value exposed makes it easier to adapt the setup for different use cases.

0 项奖励
回复