ROM Boot for NXP S32K1xx

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ROM Boot for NXP S32K1xx

2,740件の閲覧回数
gilberto_iob65
Contributor I

Some of ARM controllers have built-in bootloaders in dedicated ROM, separate from the normal flash, and can be configured to run these bootloaders before starting the application, to allow for updating the firmware without using a debug probe. How about S32k1xx devices? Is it ROM boot supported? If true, which of the available communication interfaces can be used for booting? (i.e. CA, I2C, Uart, SPI, ...).

Tks in advance for supporting

0 件の賞賛
返信
3 返答(返信)

2,667件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

there is no special ROM used for bootloader. You can flash bootloader for example at the beginning of ROM. There is bootloader example in S32 Design Studio for ARM ( S32 Design Studio for ARM 2018.R1 (Windows/Linux) released!  ) for use with RappID Boot loader utility ( https://www.nxp.com/webapp/Download?colCode=RAPPID_BOOTLOADER_UTILITY&appType=license&location=null  )

Jiri

0 件の賞賛
返信

1,443件の閲覧回数
daewoong
Contributor II
How about S32K3 ? no special ROM bootloader ?
0 件の賞賛
返信

2,667件の閲覧回数
gilberto_iob65
Contributor I

Tks for kind support

Best regards

Gilberto

0 件の賞賛
返信