RED and another two LED's are continue ON , not able flash program using openSDA /Jlink to S32K14

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RED and another two LED's are continue ON , not able flash program using openSDA /Jlink to S32K14

7,139件の閲覧回数
PU1
Contributor II

Hi,

Just started working on NXP.

facing some issue in flashing and debugging the code to this EVB . 

all other board are working.

IDE : Design Studio for ARM

I am trying to program the S32K146EVB by using openSDA  and also with the J-Link debugger

This error pop up.

the RED and Green LED's are always ON .

also tried on MATLAB example same error comes.

pu_0-1696490674188.png

 

 

0 件の賞賛
返信
5 返答(返信)

7,049件の閲覧回数
PU1
Contributor II

Hi @VaneB just tried that method,it not working.

I'm using this EVB for the flashing the code via Embedded coder of matlab and since we are not able to flash the code. so I am trying it on design studio. trying to flash example code. as per your provided link same pulse are received on that point.

0 件の賞賛
返信

7,034件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @PU1 

Does the board present this behavior from the beginning, or did it start after loading some code?

0 件の賞賛
返信

7,028件の閲覧回数
PU1
Contributor II

Hi @VaneB  

From beginning it shows same behaviour.

0 件の賞賛
返信

6,964件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @PU1 

Just to be sure, did you try the procedure mentioned in the previous shared post using OpenSDA through J7?

0 件の賞賛
返信

7,113件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @PU1 

Please refer to S32K144 in permanent reset.

Also, could you provide me with the following information? 

  • The imploded code to the devices that starts this behavior.
  • The steps you realize 
  • Any modifications made to the SW or/and HW

 

B.R.

VaneB

0 件の賞賛
返信