Project import after Git clone

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Project import after Git clone

2,834件の閲覧回数
snow3847
Contributor II

Hello,

 

I have migrated from Windows 10 to Windows 11 and reinstalled the S32 DS Software along with the Tool Packages. I have my Project in git so i cloned it and tried to import it into the Workspace. The problem is that apparently some of the configuration is not loaded correctly(?). It also says that the SDK is not compatible although i used the exact same version of last time . When i create a new project everything is good i can build and debug properly but if i try to import the project i have problems. Before reinstalling the S32DS i had no Problems also with the current Project.

 

S32DS version : v3.5

SDK version : S32k144 sdk 4.0.1

 

this is the properties window i have after i cloned the project and imported it into the Workspace (eveything is gone somehow) : 

snow3847_0-1742306119337.png

When i try to reconfigure the imported project at some point i import the sdk but cannot attach it as it says sdk version is not compatible (i used the same sdk as before for this project which is the 4.0.1)

 

i would be happy with any feedback 

Thank you for the help.

0 件の賞賛
返信
3 返答(返信)

2,811件の閲覧回数
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @snow3847,

Could you confirm if SDK 4.0.1 is correctly installed in your S32DS? 

Julin_AragnM_0-1742336058539.png

I've tested importing a Git example by simply exporting the hello_world_s32k144 project and importing it through Git:

Julin_AragnM_1-1742336112039.png

There were no issues with building it. When importing the project, is it correctly shown in the project wizard?

Julin_AragnM_2-1742336350574.png

Best regards,
Julián

0 件の賞賛
返信

2,789件の閲覧回数
snow3847
Contributor II

Hi! Thanke you for the response. Those are the packages that i have installed 

0 件の賞賛
返信

2,762件の閲覧回数
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @snow3847

Before updating to Windows 11, was the IDE used S32DS 3.5 as well? 

If you have the correct packages installed, this may be an issue with the project uploaded to the Git repository, either some files missing when cloning or other dependencies needed by it.

Are you able to share the project? 

Best regards,
Julián

0 件の賞賛
返信