Running LIN Demo and Free master together possible?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Running LIN Demo and Free master together possible?

Jump to solution
485 Views
rohans002
Contributor III

I want to use the LIN demo example and use it to demonstrate on Freemaster, I just got to know that both things use the same LPUART peripheral that inst 2.
what to do?

0 Kudos
Reply
1 Solution
461 Views
_Leo_
NXP TechSupport
NXP TechSupport

Hi,

Thank you so much for your interest in our products and for using our community.

For your previous tickets, I assume that you are using S32K144EVB. If not please tell me.

In S32K144EVB, LIN Phy is connected to LPUART2, while OpenSDA is connected to LPUART1, the last one is commonly used to connect to FreeMASTER thought the Micro USB connector.

On the other hand, you can customize SW to connect FreeMASTER to any LPUART instance or even CAN. Additionally, you can customize your HW to connect LIN Phy to any LPUART instance.

Hope it helps you.

Have a nice day!

View solution in original post

0 Kudos
Reply
1 Reply
462 Views
_Leo_
NXP TechSupport
NXP TechSupport

Hi,

Thank you so much for your interest in our products and for using our community.

For your previous tickets, I assume that you are using S32K144EVB. If not please tell me.

In S32K144EVB, LIN Phy is connected to LPUART2, while OpenSDA is connected to LPUART1, the last one is commonly used to connect to FreeMASTER thought the Micro USB connector.

On the other hand, you can customize SW to connect FreeMASTER to any LPUART instance or even CAN. Additionally, you can customize your HW to connect LIN Phy to any LPUART instance.

Hope it helps you.

Have a nice day!

0 Kudos
Reply