Program Partition

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Program Partition

2,299件の閲覧回数
andreaolivieri
Contributor I

Hi All.

I already asked this question in a previous post but I would like to put it in a dedicated tiket (See Lock up event on Flash partitioning ).

Is the "Program Partition command" a procedure which has to be execute through executable code located in RAM?

Shall I have to perform an overlay?

I'm asking so because in the device's RM (Rev. 6, 12/2017) I noticed this recommendation in § "35.5.11.14 Program Partition command" which states :

 

"...

Program Partition command must not be launched from flash memory, since flash memory resources are not accessible during Program Partition command execution.

..."

タグ(1)
0 件の賞賛
返信
1 返信

2,195件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Andrea,

You can find the statement in the latest RM rev.11 as well.

It can be launch either internally from RAM or by a programmer.

Regards,

Daniel

pastedImage_2.png

pastedImage_3.png

pastedImage_4.png

0 件の賞賛
返信