Program Partition

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Program Partition

2,320 Views
andreaolivieri
Contributor I

Hi All.

I already asked this question in a previous post but I would like to put it in a dedicated tiket (See Lock up event on Flash partitioning ).

Is the "Program Partition command" a procedure which has to be execute through executable code located in RAM?

Shall I have to perform an overlay?

I'm asking so because in the device's RM (Rev. 6, 12/2017) I noticed this recommendation in § "35.5.11.14 Program Partition command" which states :

 

"...

Program Partition command must not be launched from flash memory, since flash memory resources are not accessible during Program Partition command execution.

..."

Tags (1)
0 Kudos
Reply
1 Reply

2,216 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Andrea,

You can find the statement in the latest RM rev.11 as well.

It can be launch either internally from RAM or by a programmer.

Regards,

Daniel

pastedImage_2.png

pastedImage_3.png

pastedImage_4.png

0 Kudos
Reply