Problem with S32K148 and DP83848

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem with S32K148 and DP83848

1,645 Views
Zhangfeng1
Contributor I

I am testing a controller board, whose main chip is S32K148 and network chip is DP83848. If I want to run the LWIP protocol stack, what parts do I need to modify on the official example? What other options may need to be modified besides modifying the MII option in the tcpip component when I use RMII for communication? The circuit of DP83848 has been verified on another controller and there is no problem.

Looking forward to your reply, thank you.

0 Kudos
Reply
2 Replies

1,617 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

per my understanding no further setting would be needed. You can just check pin initialization if it corresponds to your connection.
No PHY init is done in demo, I think. PHY can be configured via strap options to run in some mode, and if it is the same with the option selected in tcpip component, no PHY init is required.

BR, Petr

0 Kudos
Reply

1,596 Views
Zhangfeng1
Contributor I
Hi
Thank you for your reply.I have checked Phy's initialization and found that the problem lies here.The problem has been solved now.
Regards
0 Kudos
Reply