Problem with S32K148 and DP83848

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem with S32K148 and DP83848

1,696件の閲覧回数
Zhangfeng1
Contributor I

I am testing a controller board, whose main chip is S32K148 and network chip is DP83848. If I want to run the LWIP protocol stack, what parts do I need to modify on the official example? What other options may need to be modified besides modifying the MII option in the tcpip component when I use RMII for communication? The circuit of DP83848 has been verified on another controller and there is no problem.

Looking forward to your reply, thank you.

0 件の賞賛
返信
2 返答(返信)

1,668件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

per my understanding no further setting would be needed. You can just check pin initialization if it corresponds to your connection.
No PHY init is done in demo, I think. PHY can be configured via strap options to run in some mode, and if it is the same with the option selected in tcpip component, no PHY init is required.

BR, Petr

0 件の賞賛
返信

1,647件の閲覧回数
Zhangfeng1
Contributor I
Hi
Thank you for your reply.I have checked Phy's initialization and found that the problem lies here.The problem has been solved now.
Regards
0 件の賞賛
返信