Problem with LPUART_ECHO

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem with LPUART_ECHO

ソリューションへジャンプ
3,190件の閲覧回数
pankajprasad100
Contributor III

HI,

 I am working with LPUART in S32K116 board, while loading example project it says that "Problem during loading"s32k116_48" component: repository URLsdk.PNG 

 

why its not loading?? 

 

 

Thanks &Regards

PANKAJ PRASAD

 

 

0 件の賞賛
返信
1 解決策
3,153件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信
5 返答(返信)
3,174件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi PANKAJ PRASAD,

The version of SDK LPUART_ECHO example seems too old.
Would you please let me know the version of S32DS that you are using?
If you are using S32 Design Studio for ARM 2.2, please import the example in S32 SDK for S32K1xx SR RTM 3.0.3.
If you are using S32 Design Studio for S32 Platform v3.4, please import the example in S32SDK S32K1xx RTM 4.0.1.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
3,169件の閲覧回数
pankajprasad100
Contributor III

Currently iam using Version: 2018.R1  and while updating it says that all are updated.

 

May i know what to do now?

 

 

 

Thanks & Regards

PANKAJ PRASAD

0 件の賞賛
返信
3,165件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Please check if you have installed the S32 Design Studio for ARM 2018.R1 - Update 11 available.

0 件の賞賛
返信
3,161件の閲覧回数
pankajprasad100
Contributor III

yes already installed

0 件の賞賛
返信
3,154件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

You can refer:

S32DS 2018 SDK 3.0.0.png

0 件の賞賛
返信