I set two Gpt channels 0 and 1, using LPIT_CH0 and LPIT_CH1 respectively, and set the GptChainMode property of LPIT_CH1 to True. Only channel 0 is started on the application, and the timeout period is 1000us, but there is no change in LPIT_CH1, and the millisecond count cannot be realized.
Hello @ou_gangxun ,
The channel 1 also need to be started on the application. Then the channel 1 's timer decrements on channel 0 's timeout pulse
Best regards,
Hung