I enabled the pins configuration tool in the default FlexCAN_Ip_Example_S32K344 to observe the CAN0 Tx output on the PTA7 pin in the normal mode. I was able to see the digital CAN signals on the oscilloscope.
But when I changed the output port from PTA7 to PTB1, I couldn't see any signals on the oscilloscope.
I also tried changing CAN0 to CAN1, but still I can only see signals from the PTA7 port.
Is there any reason why can't I observe CAN signals from any ports other than PTA7 becuase in schematics both PTA7 and PTB1 can have CAN0_Tx signal.
I am using S32K3X4EVB-T172 board have attached the project.