S32K312 initialize MPU Hardfault

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K312 initialize MPU Hardfault

1,529件の閲覧回数
Ean
Contributor II
S32K312 FREERTOS project, call Mpu_M7_Ip_Init to initialize the MPU function, run to MCAL_DATA_SYNC_BARRIER, hardfault occurs1.jpg2.jpg3.jpg4.jpg
タグ(1)
0 件の賞賛
返信
1 返信

1,506件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @Ean 

According to the provided information by the internal team. There are two FreeRTOS ports, one that includes MPU support and one that does not. The S32K3 Reference Software package contains port without MPU support. It is up to the user to port the version with MPU if needed.

 

B.R.

VaneB

0 件の賞賛
返信