Please provide a example project by using Flexio I2C with MCAL in RTD 2.0.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Please provide a example project by using Flexio I2C with MCAL in RTD 2.0.0

Jump to solution
2,822 Views
HardyUp
Contributor I

Hello,

Now I'm using RTD 2.0.0 to configure a flexio I2C MCAL project but it doesn't work normally(ChannelStatus is not correctly).

Can you project a example project that I can refer, thanks!

0 Kudos
Reply
1 Solution
2,735 Views
DanNguyenDuy
NXP Employee
NXP Employee

Dear HardyUp,

Sorry because my response is quite late. This attachment file is my example using Flexio I2C with MCAL in RTD 2.0.0

Best regards,

Dan

View solution in original post

0 Kudos
Reply
4 Replies
2,720 Views
HardyUp
Contributor I

Dear Dan,

I also see it in RTD 2.0.0 example projects. The description.txt file made me regrad it as Driver project.

Anyway, thanks for your reply.

 

Best Regrads

0 Kudos
Reply
2,805 Views
DanNguyenDuy
NXP Employee
NXP Employee

Dear HardyUp,

Could you provide me with the driver's name, you are using?

(for example: SW32K3_RTD_4.4_2.0.0_CD01)

Best regards,

Dan

0 Kudos
Reply
2,801 Views
HardyUp
Contributor I

Hi Dan,

I upgraded RTD from 1.0.0 to 2.0.0 by DS32 update item.

In disk C it shows "C:\NXP\S32DS.3.4\S32DS\software\PlatformSDK_S32K3_2022_03\SW32K3_RTD_4_4_2_0_0_D2203"

The version should be same with NXP website "SW32K3_RTD_4.4_2.0.0_DS_updatesite_D2204".

 

Issue description is in attachment, please refer, thanks a lot!

 

0 Kudos
Reply
2,736 Views
DanNguyenDuy
NXP Employee
NXP Employee

Dear HardyUp,

Sorry because my response is quite late. This attachment file is my example using Flexio I2C with MCAL in RTD 2.0.0

Best regards,

Dan

0 Kudos
Reply