Please provide a example project by using Flexio I2C with MCAL in RTD 2.0.0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Please provide a example project by using Flexio I2C with MCAL in RTD 2.0.0

跳至解决方案
2,821 次查看
HardyUp
Contributor I

Hello,

Now I'm using RTD 2.0.0 to configure a flexio I2C MCAL project but it doesn't work normally(ChannelStatus is not correctly).

Can you project a example project that I can refer, thanks!

0 项奖励
回复
1 解答
2,734 次查看
DanNguyenDuy
NXP Employee
NXP Employee

Dear HardyUp,

Sorry because my response is quite late. This attachment file is my example using Flexio I2C with MCAL in RTD 2.0.0

Best regards,

Dan

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,719 次查看
HardyUp
Contributor I

Dear Dan,

I also see it in RTD 2.0.0 example projects. The description.txt file made me regrad it as Driver project.

Anyway, thanks for your reply.

 

Best Regrads

0 项奖励
回复
2,804 次查看
DanNguyenDuy
NXP Employee
NXP Employee

Dear HardyUp,

Could you provide me with the driver's name, you are using?

(for example: SW32K3_RTD_4.4_2.0.0_CD01)

Best regards,

Dan

0 项奖励
回复
2,800 次查看
HardyUp
Contributor I

Hi Dan,

I upgraded RTD from 1.0.0 to 2.0.0 by DS32 update item.

In disk C it shows "C:\NXP\S32DS.3.4\S32DS\software\PlatformSDK_S32K3_2022_03\SW32K3_RTD_4_4_2_0_0_D2203"

The version should be same with NXP website "SW32K3_RTD_4.4_2.0.0_DS_updatesite_D2204".

 

Issue description is in attachment, please refer, thanks a lot!

 

0 项奖励
回复
2,735 次查看
DanNguyenDuy
NXP Employee
NXP Employee

Dear HardyUp,

Sorry because my response is quite late. This attachment file is my example using Flexio I2C with MCAL in RTD 2.0.0

Best regards,

Dan

0 项奖励
回复