Please provide a example project by using Flexio I2C with MCAL in RTD 2.0.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Please provide a example project by using Flexio I2C with MCAL in RTD 2.0.0

ソリューションへジャンプ
2,879件の閲覧回数
HardyUp
Contributor I

Hello,

Now I'm using RTD 2.0.0 to configure a flexio I2C MCAL project but it doesn't work normally(ChannelStatus is not correctly).

Can you project a example project that I can refer, thanks!

0 件の賞賛
返信
1 解決策
2,792件の閲覧回数
DanNguyenDuy
NXP Employee
NXP Employee

Dear HardyUp,

Sorry because my response is quite late. This attachment file is my example using Flexio I2C with MCAL in RTD 2.0.0

Best regards,

Dan

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,777件の閲覧回数
HardyUp
Contributor I

Dear Dan,

I also see it in RTD 2.0.0 example projects. The description.txt file made me regrad it as Driver project.

Anyway, thanks for your reply.

 

Best Regrads

0 件の賞賛
返信
2,862件の閲覧回数
DanNguyenDuy
NXP Employee
NXP Employee

Dear HardyUp,

Could you provide me with the driver's name, you are using?

(for example: SW32K3_RTD_4.4_2.0.0_CD01)

Best regards,

Dan

0 件の賞賛
返信
2,858件の閲覧回数
HardyUp
Contributor I

Hi Dan,

I upgraded RTD from 1.0.0 to 2.0.0 by DS32 update item.

In disk C it shows "C:\NXP\S32DS.3.4\S32DS\software\PlatformSDK_S32K3_2022_03\SW32K3_RTD_4_4_2_0_0_D2203"

The version should be same with NXP website "SW32K3_RTD_4.4_2.0.0_DS_updatesite_D2204".

 

Issue description is in attachment, please refer, thanks a lot!

 

0 件の賞賛
返信
2,793件の閲覧回数
DanNguyenDuy
NXP Employee
NXP Employee

Dear HardyUp,

Sorry because my response is quite late. This attachment file is my example using Flexio I2C with MCAL in RTD 2.0.0

Best regards,

Dan

0 件の賞賛
返信