Parsing Error while importing ldf

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Parsing Error while importing ldf

1,913件の閲覧回数
Sumit1729
Contributor I

Hi Folks,

i am trying to integrate ldf file into projects but its throwing error "Parse lin description file fails. Do you want to create new content files." i have gone through the topics already available on the forum but it did not helped me out. Attached is the ldf file, please check it out if it has some problems. i need to generate the code from the attached LDF using S32DS. Please check it out, its an urgent topic. Any suggestion is appreciated.

Thanks.

#LDF_Parsing_Error #S32DS #S32K #S32K116F128M4

0 件の賞賛
返信
1 返信

1,864件の閲覧回数
DanNguyenDuy
NXP Employee
NXP Employee

Hi Sumit1729,

The attachment is the corrected ldf file.

Best regards,

Dan

0 件の賞賛
返信