Package Installation Issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Package Installation Issue

1,779 Views
Joseph_David
Contributor I

Hello all,  
      I am working with the S32K148 Microcontroller. While I am installing the Packages in S32DS, I am unable to install those packages. I am getting the error as shown in the picture. Help me with this.

Joseph_David_0-1745989897144.pngJoseph_David_0-1745989897144.png

 

 

0 Kudos
Reply
4 Replies

1,747 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Are you installing S32K1 SDK or RTD?
Please refer to the third step of HOWTO: offline install S32K1 RTD 2.0.0 in S32DS v3.5
This includes NXP GCC for Arm Embedded Processors v10.2 build 1728


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

1,694 Views
Joseph_David
Contributor I

I have installed everything as mentioned in https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-offline-install-S32K1-RTD-2-0-0-... . After Installing I tried to build example project and I got errors as Header Files Missing. It is happening with all example projects. Help me with this.

0 Kudos
Reply

1,677 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Please follow the description.txt of the project. Did you click on the "S32 Configuration Tool->Update Code" button?

3. Generating, building and running the example application

3.1 Generating the S32 configuration

Before running the example a configuration needs to be generated. First go to Project Explorer View in S32 DS and select the current project.

Select the "S32 Configuration Tool" menu then click on the desired configuration tool (Pins, Clocks, Peripherals etc...).

Clicking on any one of those will generate all the components.

Make the desired changes (if any) then click on the "S32 Configuration Tool->Update Code" button.

0 Kudos
Reply

1,735 Views
Joseph_David
Contributor I

Thanks for your reply. I’ve installed everything you mentioned.  I'm currently working on a Battery Management System (BMS).
      If you know of any reference projects for a BMS using the S32K148 microcontroller (S32K148_LQFP 176 package), I’d really appreciate it if you could share them.

0 Kudos
Reply