PMC&CMU Error Injection

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PMC&CMU Error Injection

Jump to solution
3,394 Views
Pusoy
Contributor III

Hi,

Recently, I have been using the PMC and CMU modules, but I haven't found a way to inject related exceptions to validate my program logic.


1. For the PMC module, is there a way to inject voltage exceptions? (such as injecting high or low voltage exceptions for VDD_HV_A)
2. For the CMU module, is there a way to inject frequency exceptions? (such as injecting high or low frequency exceptions for CMU_FC0)


Thank you very much!

Tags (4)
0 Kudos
Reply
1 Solution
3,275 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

No PMC nor CMU injection is possible here. Nor required.

This is all covered by SAF:

petervlna_0-1704366956686.png

refer to safety manual for more details.

Best regards,

Peter

View solution in original post

0 Kudos
Reply
4 Replies
3,355 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

on certain microcotrollers there is, but please specify the device you are using.

Best regards,

Peter

0 Kudos
Reply
3,293 Views
Pusoy
Contributor III

Hello,

I have a development board based on the S32K344 chip, with the model S32K3x4_HDQFP172, as shown in the picture below.

1704280715718.jpg

Additionally, I also have a chip S32K312. 

1. Can these two devices inject PMC&CMU errors? If so, please provide the methods.

Thank you very much, I am looking for your replay!

0 Kudos
Reply
3,276 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

No PMC nor CMU injection is possible here. Nor required.

This is all covered by SAF:

petervlna_0-1704366956686.png

refer to safety manual for more details.

Best regards,

Peter

0 Kudos
Reply
3,353 Views
Pusoy
Contributor III

I am using S32K344 MQFP172

0 Kudos
Reply