PINS_DRV_Init => No source available for "__isr_vector() at 0x0"

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PINS_DRV_Init => No source available for "__isr_vector() at 0x0"

3,264 次查看
MaxSKDRN
Contributor II

Hello

I've an issue with debugging :

calling "PINS_DRV_Init(NUM_OF_CONFIGURED_PINS0, g_pin_mux_InitConfigArr0);"
I'm getting disconnected from debug with "No source available for "__isr_vector() at 0x0" screen
The software on the S32KEVB still run without issue but I can't use debugger

The disconnection append in file "pin_port_hw_access.c",
In the function "void PINS_Init(const pin_settings_config_t * config)"
on the line "config->base->PCR[config->pinPortIdx] = regValue;"
for the 7th pin (previous pins are initialized without debugger disconnection)

It's seems to be PTC4, used for FTM1/ch0 peripheral

Any idea why I'm getting disconnectied from debugging, and how to avoir this ?

Thanks

Maxime

{
.base = PORTC,
.pinPortIdx = 4U,
.pullConfig = PORT_INTERNAL_PULL_DOWN_ENABLED,
.driveSelect = PORT_LOW_DRIVE_STRENGTH,
.passiveFilter = false,
.mux = PORT_MUX_ALT2,
.pinLock = false,
.intConfig = PORT_DMA_INT_DISABLED,
.clearIntFlag = false,
.gpioBase = NULL,
.digitalFilter = false,
},

 

0 项奖励
回复
1 回复

3,252 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Maxime,

PTC4 is default as debug pins(JTAG_TCLK / SWD_CLK), if you change it FTM1_CH0, then the debug connection will be error.
Did you consider use PTB2 as FTM1_CH0?

PTC4 alt2 FTM1_CH0.pngPTC4 JTAG_TCLK SWD_CLK.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复