PCS value can't be modified in generated code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCS value can't be modified in generated code

2,247 Views
zp001
Contributor III

Hi NXP exports,

The PCS value can't be generated by EB, and I have double checked SPi configuration is right.

zp001_0-1639985649872.png

but actual code ,the PCS is always 0.

zp001_1-1639985692569.png

 

 

0 Kudos
Reply
4 Replies

2,226 Views
namnguyenviet
NXP Employee
NXP Employee

Hello @zp001,

Could you share the configuration file (in epc or arxml)? Which MCAL package are you using?

Best Regards,

Nam

0 Kudos
Reply

2,217 Views
zp001
Contributor III

Hello Nam,

SPI configuration files have been uploaded, please help us check!

Thanks a lot!

0 Kudos
Reply

2,188 Views
namnguyenviet
NXP Employee
NXP Employee

Hello @zp001,

Please enable the SpiCsSelection, and then select CS_VIA_PERIPHERAL_ENGINE:

namnguyenviet_0-1640587590351.png

After that, I can see PCS had value:

namnguyenviet_1-1640587639333.png

Best Regards,

Nam

 

 

0 Kudos
Reply

2,182 Views
zp001
Contributor III

Hi Nam, Appreciate your support! Thanks!

0 Kudos
Reply