OTA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OTA

10,562 Views
814420552
Contributor III

hello,

Does S32K1xx have OTA function? How to use OTA function? Is there a document for reference?

wish  your help?

0 Kudos
Reply
13 Replies

10,394 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport
0 Kudos
Reply

10,394 Views
814420552
Contributor III

hello Lukas, 

   As of today, I have read the OTA document you sent. How can I put bootloader into d-flash?

about OTA Another problem is In the example you gave me, I can see that the current app will pause when upgrading how to upgrade the app code while running itThat is, the upgrade does not affect the current app operation)?  

thanks in advance!

0 Kudos
Reply

10,395 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Kui,

to put the bootloader to specific area, you need to change the linker file. You can check this file:

..\AN12323SW.zip\AN_S32K_OTA\OTA_S32K146_Use_Case_WS\S32K146_FOTA_Bootloader\Project_Settings\Linker_Files\S32K1xx_flexnvm.ld

If you want to keep your application running when updating new firmware, important point is that you need a microcontroller with more partitions in code flash, so you can execute your firmware from one partition while another one is being updated. That means either S32K146 or S32K148.

S32K144 (or all S32K11x) have only single partition in case of code flash.

The procedure is thoroughly explained in chapter "6.2 S32K146 use case". Please read whole chapter, especially description of SCENARIO (1) and SCENARIO (2).

Regards,

Lukas

0 Kudos
Reply

10,395 Views
814420552
Contributor III

Dear lukas

   1. if bootloader save in D-Flash ,it seems  that it is conflict with  the following function.

   2. when update firmware,  how does the code jump between APP & bootloader?

pastedImage_1.png

0 Kudos
Reply

10,395 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Kui,

1. Yes, there are two partitions in S32K146, so it supports updating of one partition while the other is being updated.

2. I wrote that it is supported:

"If you want to keep your application running when updating new firmware, important point is that you need a microcontroller with more partitions in code flash, so you can execute your firmware from one partition while another one is being updated. That means either S32K146 or S32K148."

3. S32K146 implements scenario 2.

4. Yes, secure boot always uses start address 0. But the bootloader can be still protected by secure boot. It can be relatively easily solved by chain of trust. You can place simple piece of code to the first sector of flash. This can be protected directly by secure boot. This piece of code then can check CMAC of the bootloader in D-Flash. If it is correct, jump to the bootloader.

5. Simply use function pointer. It's shown in the demo codes.

Regards,

Lukas

0 Kudos
Reply

10,395 Views
814420552
Contributor III

hello Lukas.

   5. Simply use function pointer. It's shown in the demo codes.

   S32K146 implements scenario 2, it need jump between APP and bootloader untill Firmware updated complete.

  Step 1. every time when received the update firmware data , code jump from APP to bootloader and execute from the first line code if main function, then write the new foreware to anther bank.  every time code will call the init function in bootloader.

  

 Step 2

   of course evevy time when wrote  new fireware data completely, code will jump to APP  for handing user's application & receiving the new fireware data.  code will also  do init work then run to while 1 in main function. 

if my understanding right?

thus  ervey time for jumping from APP to bootloader or jumping from bootloader to APP, bootloader or APP  will do init work 

  

0 Kudos
Reply

10,395 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

The zip package contain demo code for S32K146 and it's for scenario 2.

Take a look at the code, not complete initialization is done. Only some specific functions are called.

Regards,

Lukas

0 Kudos
Reply

10,395 Views
814420552
Contributor III

hello lukas,

   I still can't find the code which jump to bootloader from app in demo code, could you tell me which line code do this jump?

  I still have a doublt,  when jump every time, it should save the PC pointer and stack, when return it will restore the PC and stack.  is my understanding wrong?

thanks very much!

0 Kudos
Reply

10,395 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Kui,

well, I can see now that there are only binaries of the application.

But if you take closer look at the bootloader, you can see in linker file:

pastedImage_1.png

And then in main.c:

pastedImage_2.png

and

pastedImage_3.png

So, address 0x10003FFC contains pointer to function which you should call from application and address 0x2000EFFC contains status (return value) of that function which you are supposed to read after return.

In application, simply create a pointer to function:

void (*f_ptr)(void);

Load content of address 0x10003FFC  to the pointer:

f_ptr = (void(*)(void))(*(unsigned int*)0x10003FFC);

And call the function:

f_ptr();

When you return from the function, simply read status from 0x2000EFFC using a pointer.

You do not need to save/restore register content because you are still using C and EABI.

Regards,

Lukas

0 Kudos
Reply

10,395 Views
814420552
Contributor III

hello Lukas,   

   3. S32K146 implements scenario 2. 

   I have the dmo for scenario 1.

   whether could you send the demo (scenario 2) code for me?  

   thanks very much!

0 Kudos
Reply

10,395 Views
814420552
Contributor III

hello Lukas,   

   3. S32K146 implements scenario 2.

   whether could you send the demo code for me?  

   thanks very much!

0 Kudos
Reply

10,395 Views
814420552
Contributor III

Hello Lukas, 

      <1>My device is S32K146, according to reference manual, it should be support two partition for P-Flash?  is my understanding wrong as the following picture description?

     <2>As the last mail your description, S32K146 or 148 can not support application running when updating new firmware??

     <3>which SCENARIO (chapter "6.2 S32K146 use case".  SCENARIO (1)  and SCENARIO (2) )does the OTA demo code for in https://www.nxp.com/docs/en/application-note-software/AN12323SW.zip  ???  if this demo code fufil SCENARIO (1), thus whether has the demo code for SCENARIO (2)?

     thank for your anser!

pastedImage_1.png

0 Kudos
Reply

10,392 Views
814420552
Contributor III

hello Lukas, 

      My device is S32K146, according to reference manual, it should be support two partition for P-Flash?  is my understanding wrong as the following picture description?

     As the last mail your description, S32K146 or 148 can not support application running when updating new firmware??

     thank for your anser!

pastedImage_1.png

0 Kudos
Reply