Not able to test S32K142 Lin Slave sample code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Not able to test S32K142 Lin Slave sample code

ソリューションへジャンプ
2,836件の閲覧回数
sivaEmbitel
Contributor II

Hi

I am using S32K142EVB Evaluation Board – REV.

I am unable to communicate Lin slave example code (both lin_slave_baremetal_s32k142 and lin_slave_s32k142).

Please let me know the Hardware connection and necessary Software changes to make it work (for lin_slave_baremetal_s32k142 example code).

 

Thanks in advance.

 

 

 

 

0 件の賞賛
返信
1 解決策
2,795件の閲覧回数
sivaEmbitel
Contributor II

Hi Daniel,

Thanks for your reply,

I am able to test the sample code after some workaround between J4 and J6 instead of J5 and J6

J6-9 (\b PTD6) - J4-5 (\b PTC8)  ----- Rx pin

J6-11 (\b PTD7) - J4-7 (\b PTC9) ------ Tx pin

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,812件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @sivaEmbitel,

the lin_slave_baremetal_s32k142 example works with the lin_master_baremetal_s32k142 example.

If you have two boards, you can connect them via LIN and communicate.

This is explained in the description of the two examples, please find the description in the S32DS installation directory

For example:

file:///C:/NXP/S32DS.3.4/S32DS/software/S32SDK_S32K1XX_RTM_4.0.2/doc/html_S32K142/lin_master_baremet...

file:///C:/NXP/S32DS.3.4/S32DS/software/S32SDK_S32K1XX_RTM_4.0.2/doc/html_S32K142/lin_slave_baremeta...

danielmartynek_0-1643810482378.pngdanielmartynek_0-1643810482378.png

 

danielmartynek_1-1643810521407.pngdanielmartynek_1-1643810521407.png

 

Regards,

Daniel

 

 

 

0 件の賞賛
返信
2,796件の閲覧回数
sivaEmbitel
Contributor II

Hi Daniel,

Thanks for your reply,

I am able to test the sample code after some workaround between J4 and J6 instead of J5 and J6

J6-9 (\b PTD6) - J4-5 (\b PTC8)  ----- Rx pin

J6-11 (\b PTD7) - J4-7 (\b PTC9) ------ Tx pin

0 件の賞賛
返信