hi,
Blocksize here refers to the number of frames sent in between the Flow control frames.
Blocksize is hardcoded inside the software. Based on the Blocksize it will transfer the data.
For Example:
1. If the Blocksize is one
During Transfer data request, the Boot loader will send first 8 bytes and waits for the flow control frame. If it receives the flow control frame then it sends the next 8 bytes of data.
2. If the Blocksize is two
It will send two 8 bytes of data and waits for flow control frame, if the Flow control frame is received it will send the next two 8 bytes of data.