S32K GPIO output Voh=? range at 5.0v with 0-5mA current.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K GPIO output Voh=? range at 5.0v with 0-5mA current.

2,127 次查看
jacky_Tan
NXP Employee
NXP Employee

s32k_GPIO.png

标签 (1)
0 项奖励
回复
3 回复数

2,000 次查看
jacky_Tan
NXP Employee
NXP Employee

thank you Daniel,

would you please provide that customer needs to know the voltage if the pin is loaded with 0mA? no this data in the S32K1xx datasheet.

0 项奖励
回复

2,000 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Jacky,

The output is driven to VDD or VSS.

If the pin is not loaded, the sink/source current is 0mA, the output is equal to VDD or VSS.

Regards,

Daniel

2,000 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Jacky,

What is the question here?

The specification says that the voltage drops to VDD - 0.8V when the pin is loaded with 5 mA.

Regards,

Daniel

0 项奖励
回复