Need information regarding MCU

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Need information regarding MCU

912件の閲覧回数
pratayay123
Contributor III

what is the operating voltage of the input ADC pin ..0-3.3 volt or 0-5 volt?

0 件の賞賛
返信
1 返信

907件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

you did not specify the MCU, lets assume S32K144.
ADC input should be between VREFL and VREFH. Recommended condition is to have VDD=VDDA=VREFH. Anyway VDDA and VDD must be shorted on PCB, but VREFH can be connected to another source. And there is a restriction, VREFH should be equal or less than VDDA + 0.1V and VDD + 0.1V.

BR, Petr

0 件の賞賛
返信