Need information regarding MCU

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Need information regarding MCU

1,314 次查看
pratayay123
Contributor III

what is the operating voltage of the input ADC pin ..0-3.3 volt or 0-5 volt?

0 项奖励
回复
1 回复

1,309 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

you did not specify the MCU, lets assume S32K144.
ADC input should be between VREFL and VREFH. Recommended condition is to have VDD=VDDA=VREFH. Anyway VDDA and VDD must be shorted on PCB, but VREFH can be connected to another source. And there is a restriction, VREFH should be equal or less than VDDA + 0.1V and VDD + 0.1V.

BR, Petr

0 项奖励
回复