NBP8 false Pins

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NBP8 false Pins

Jump to solution
2,384 Views
Khaledag
Contributor II

Hi, 

I'm trying to program the NBP8 over SPI with an NXP S32K146 and a strange thing is happening. The Sensor is connected correctly but the clock signal is coming out of the MOSI pin and the MOSI signal comes out of the clock pin.
Also one strange thing the uC is doing is turning on the blue LED on D11 when the code is running. 
If I take the sensor down and still look at the scope I still find it false. 

Any Idea whats happening?

 

I'm Using LPSPI1 over PORTD 

Tags (3)
0 Kudos
Reply
1 Solution
2,309 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @Khaledag 

According to the Pin configuration share. There is a discrepancy between PTD0 and PTD2. 

As shown in your code you mark these pins as LPSPI1_SOUT (PTD0) and LPSPI1_SCK (PTD2).

 

PORTD->PCR[2]|=PORT_PCR_MUX(3); /* MUX = ALT3, LPSPI1_SCK */
PORTD->PCR[1]|=PORT_PCR_MUX(3); /* MUX = ALT3, LPSPI1_SIN */
PORTD->PCR[0]|=PORT_PCR_MUX(3); /* MUX = ALT3, LPSPI1_SOUT */
PORTD->PCR[3]|=PORT_PCR_MUX(3); /* MUX = ALT3, LPSPI1_PCS3 */

 

But if we refer to the S32K146 IO_Signal_Description_Input_Multiplexing (attached to the reference manual) PTD0 is LPSPI1_SCK and PTD2 is LPSPI1_SOUT.

VaneB_0-1711560234774.pngVaneB_0-1711560234774.png

So, "coming out of the MOSI pin and the MOSI signal comes out of the clock pin" the situation is the correct behavior. 

View solution in original post

0 Kudos
Reply
3 Replies
2,365 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @Khaledag 

Could you share your SPI and pin configurations? 

Also, I assume that when you said NXP S32K146 you refer to the EVB, is my understanding correct?

 

B.R.

VaneB

0 Kudos
Reply
2,319 Views
Khaledag
Contributor II

Hey, sorry for the late reply.
 Yes I'm using the EVB

SPI looks like this with these pins: 

 

/*
 * Copyright (c) 2014 - 2016, Freescale Semiconductor, Inc.
 * Copyright (c) 2016 - 2018, NXP.
 * All rights reserved.
 *
 * Redistribution and use in source and binary forms, with or without
 * modification, are permitted provided that the following conditions are met:
 *
 * 1. Redistributions of source code must retain the above copyright notice,
 *    this list of conditions and the following disclaimer.
 *
 * 2. Redistributions in binary form must reproduce the above copyright notice,
 *    this list of conditions and the following disclaimer in the documentation
 *    and/or other materials provided with the distribution.
 *
 * 3. Neither the name of the copyright holder nor the names of its contributors
 *    may be used to endorse or promote products derived from this software
 *    without specific prior written permission.
 *
 * THIS SOFTWARE IS PROVIDED BY NXP "AS IS" AND ANY EXPRESSED OR
 * IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES
 * OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED.
 * IN NO EVENT SHALL NXP OR ITS CONTRIBUTORS BE LIABLE FOR ANY DIRECT,
 * INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES
 * (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR
 * SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION)
 * HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT,
 * STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING
 * IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF
 * THE POSSIBILITY OF SUCH DAMAGE.
 */

#include "device_registers.h"	  /* include peripheral declarations */
#include <stdio.h>

void LPSPI1_init_master(void)
{
	/*!
	 * LPSPI1 Clocking:
	 * ===================================================
	 */
	PCC->PCCn[PCC_LPSPI1_INDEX] = 0;          		/* Disable clocks to modify PCS ( default) 	*/
	PCC->PCCn[PCC_LPSPI1_INDEX] = PCC_PCCn_PR_MASK	/* (default) Peripheral is present.			*/
								 |PCC_PCCn_CGC_MASK	/* Enable PCS=SPLL_DIV2 (40 MHz func'l clock) 	*/
								 |PCC_PCCn_PCS(6);
	/*!
	 * LPSPI1 Initialization:
	 * ===================================================
	 */
  LPSPI1->CR    = 0x00000000;   			/* Disable module for configuration 			*/
  LPSPI1->IER   = 0x00000000;   			/* Interrupts not used 						*/
  LPSPI1->DER   = 0x00000000;   			/* DMA not used 								*/
  LPSPI1->CFGR0 = 0x00000000;   			/* Defaults: 									*/
                                			/* RDM0=0: rec'd data to FIFO as normal 		*/
                                			/* CIRFIFO=0; Circular FIFO is disabled 		*/
                                			/* HRSEL, HRPOL, HREN=0: Host request disabled */

  LPSPI1->CFGR1 = LPSPI_CFGR1_MASTER_MASK;  /* Configurations: master mode									*/
											/* PCSCFG=0: PCS[3:2] are enabled 								*/
											/* OUTCFG=0: Output data retains last value when CS negated	*/
											/* PINCFG=0: SIN is input, SOUT is output 						*/
											/* MATCFG=0: Match disabled 									*/
											/* PCSPOL=0: PCS is active low 								*/
											/* NOSTALL=0: Stall if Tx FIFO empty or Rx FIFO full 			*/
											/* AUTOPCS=0: does not apply for master mode 					*/
											/* SAMPLE=0: input data sampled on SCK edge 					*/
											/* MASTER=1: Master mode 										*/

  LPSPI1->TCR   =
//		  	  	  LPSPI_TCR_CPHA_MASK
				  LPSPI_TCR_PRESCALE(2)
				  |LPSPI_TCR_PCS(3)
				  |LPSPI_TCR_FRAMESZ(15);   /* Transmit cmd: PCS3, 16 bits, prescale func'l clk by 4, etc	*/
											/* CPOL=0: SCK inactive state is low 							*/
											/* CPHA=1: Change data on SCK lead'g, capture on trail'g edge	*/
											/* PRESCALE=2: Functional clock divided by 2**2 = 4 			*/
											/* PCS=3: Transfer using PCS3 									*/
											/* LSBF=0: Data is transfered MSB first 						*/
											/* BYSW=0: Byte swap disabled 									*/
											/* CONT, CONTC=0: Continuous transfer disabled 				*/
											/* RXMSK=0: Normal transfer: rx data stored in rx FIFO 		*/
											/* TXMSK=0: Normal transfer: data loaded from tx FIFO 			*/
											/* WIDTH=0: Single bit transfer 								*/
											/* FRAMESZ=15: # bits in frame = 15+1=16 						*/

  LPSPI1->CCR   = LPSPI_CCR_SCKPCS(4)
				  |LPSPI_CCR_PCSSCK(4)
				  |LPSPI_CCR_DBT(8)
				  |LPSPI_CCR_SCKDIV(8);   	/* Clock dividers based on prescaled func'l clk of 100 nsec 	*/
											/* SCKPCS=4: SCK to PCS delay = 4+1 = 5 (500 nsec) 			*/
											/* PCSSCK=4: PCS to SCK delay = 9+1 = 10 (1 usec) 				*/
											/* DBT=8: Delay between Transfers = 8+2 = 10 (1 usec) 			*/
											/* SCKDIV=8: SCK divider =8+2 = 10 (1 usec: 1 MHz baud rate) 	*/

//  LPSPI1->FCR   = LPSPI_FCR_TXWATER(3);   	/* RXWATER=0: Rx flags set when Rx FIFO >0 	*/
                                			/* TXWATER=3: Tx flags set when Tx FIFO <= 3 	*/

  LPSPI1->CR    = LPSPI_CR_MEN_MASK
		  	  	  |LPSPI_CR_DBGEN_MASK;   	/* Enable module for operation 			*/
											/* DBGEN=1: module enabled in debug mode 	*/
											/* DOZEN=0: module enabled in Doze mode 	*/
											/* RST=0: Master logic not reset 			*/
											/* MEN=1: Module is enabled 				*/
}


void LPSPI1_transmit_16bits (uint16_t send)
{
  while((LPSPI1->SR & LPSPI_SR_TDF_MASK)>>LPSPI_SR_TDF_SHIFT==0);
                                   /* Wait for Tx FIFO available 	*/
  LPSPI1->TDR = send;              /* Transmit data 				*/
  LPSPI1->SR |= LPSPI_SR_TDF_MASK; /* Clear TDF flag 				*/
}

uint16_t LPSPI1_receive_16bits (void)
{
  uint16_t recieve = 0;

  while((LPSPI1->SR & LPSPI_SR_RDF_MASK)>>LPSPI_SR_RDF_SHIFT==0);
                                   /* Wait at least one RxFIFO entry 	*/
  recieve= LPSPI1->RDR;            /* Read received data 				*/
  LPSPI1->SR |= LPSPI_SR_RDF_MASK; /* Clear RDF flag 					*/
//  printf("%d\n", recieve);
  return recieve;                  /* Return received data 			*/
}

 

and the pins: 

 

void PORT_init (void)
{
	/*!
	 * Pins definitions
	 * ===================================================
	 *
	 * Pin number        | Function
	 * ----------------- |------------------
	 * PTB14             | LPSPI1_SCK
	 * PTB15             | LPSPI1_SIN
	 * PTB16			 | LPSPI1_SOUT
	 * PTB17			 | LPSPI1_PCS3
	 */
  PCC->PCCn[PCC_PORTD_INDEX ]|=PCC_PCCn_CGC_MASK; /* Enable clock  */
  PORTD->PCR[2]|=PORT_PCR_MUX(3); /* MUX = ALT3, LPSPI1_SCK */
  PORTD->PCR[1]|=PORT_PCR_MUX(3); /* MUX = ALT3, LPSPI1_SIN */
  PORTD->PCR[0]|=PORT_PCR_MUX(3); /* MUX = ALT3, LPSPI1_SOUT */
  PORTD->PCR[3]|=PORT_PCR_MUX(3); /* MUX = ALT3, LPSPI1_PCS3 */
}

 

 

Thanks

0 Kudos
Reply
2,310 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @Khaledag 

According to the Pin configuration share. There is a discrepancy between PTD0 and PTD2. 

As shown in your code you mark these pins as LPSPI1_SOUT (PTD0) and LPSPI1_SCK (PTD2).

 

PORTD->PCR[2]|=PORT_PCR_MUX(3); /* MUX = ALT3, LPSPI1_SCK */
PORTD->PCR[1]|=PORT_PCR_MUX(3); /* MUX = ALT3, LPSPI1_SIN */
PORTD->PCR[0]|=PORT_PCR_MUX(3); /* MUX = ALT3, LPSPI1_SOUT */
PORTD->PCR[3]|=PORT_PCR_MUX(3); /* MUX = ALT3, LPSPI1_PCS3 */

 

But if we refer to the S32K146 IO_Signal_Description_Input_Multiplexing (attached to the reference manual) PTD0 is LPSPI1_SCK and PTD2 is LPSPI1_SOUT.

VaneB_0-1711560234774.pngVaneB_0-1711560234774.png

So, "coming out of the MOSI pin and the MOSI signal comes out of the clock pin" the situation is the correct behavior. 

0 Kudos
Reply