Missing MCAL header files after EB Tresos code generation for S32K312

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Missing MCAL header files after EB Tresos code generation for S32K312

ソリューションへジャンプ
115件の閲覧回数
Matrix32
Contributor I

Hello,

I'm currently working on a project for S32K312. I've used EB Tresos (version 29.0.0) to generate AUTOSAR configuration files, and after copying these generated files into my S32 Design Studio project I see multiple errors related to missing header files.

Matrix32_0-1754426698138.png

Could someone please tell me where I can obtain these header files and can I make EB Tresos tool generate them properly along with other files?

 

Best regards,

タグ(4)
0 件の賞賛
返信
1 解決策
95件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Please follow the instructions in this article: [S32K3 Tools Part]How to import RTD EB project into S32DS


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
96件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Please follow the instructions in this article: [S32K3 Tools Part]How to import RTD EB project into S32DS


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信