Missing Directory in an Example code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Missing Directory in an Example code

ソリューションへジャンプ
2,311件の閲覧回数
akhilranga
Contributor IV

Hello there. I am new in this space. And trying to find my ropes here. I am following a s32k144 cookbook to get familar to the s32 design studio application and s32k144 board. And i have encountered the following error. Can any suggest me, how to resolve this. Is there any way i can add that missing file

Screenshot (118).pngScreenshot (118).png

Thank in advance. Would really appriciate it

#s32k144

 

タグ(1)
0 件の賞賛
返信
1 解決策
2,305件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@akhilranga

 Have you added the clocks_and_modes.c & clock_and_modes.h to your project?

Senlent_0-1657677006013.pngSenlent_0-1657677006013.png

if no, you need to add these file to your project.

if yes,you may forget to add these file path,you can take a look at this post.

https://community.nxp.com/t5/S32K/S32K-S32DS-project-name-path-and-build-problem/td-p/1260029 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,306件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@akhilranga

 Have you added the clocks_and_modes.c & clock_and_modes.h to your project?

Senlent_0-1657677006013.pngSenlent_0-1657677006013.png

if no, you need to add these file to your project.

if yes,you may forget to add these file path,you can take a look at this post.

https://community.nxp.com/t5/S32K/S32K-S32DS-project-name-path-and-build-problem/td-p/1260029 

0 件の賞賛
返信
2,300件の閲覧回数
akhilranga
Contributor IV

Hello thee,

I didn't add them in my project. Hoping those files are available in NXP resources. May i know the process to add them in my project.

Thank You 

0 件の賞賛
返信