Missing Directory in an Example code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Missing Directory in an Example code

Jump to solution
2,314 Views
akhilranga
Contributor IV

Hello there. I am new in this space. And trying to find my ropes here. I am following a s32k144 cookbook to get familar to the s32 design studio application and s32k144 board. And i have encountered the following error. Can any suggest me, how to resolve this. Is there any way i can add that missing file

Screenshot (118).pngScreenshot (118).png

Thank in advance. Would really appriciate it

#s32k144

 

Tags (1)
0 Kudos
Reply
1 Solution
2,308 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@akhilranga

 Have you added the clocks_and_modes.c & clock_and_modes.h to your project?

Senlent_0-1657677006013.pngSenlent_0-1657677006013.png

if no, you need to add these file to your project.

if yes,you may forget to add these file path,you can take a look at this post.

https://community.nxp.com/t5/S32K/S32K-S32DS-project-name-path-and-build-problem/td-p/1260029 

View solution in original post

0 Kudos
Reply
2 Replies
2,309 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@akhilranga

 Have you added the clocks_and_modes.c & clock_and_modes.h to your project?

Senlent_0-1657677006013.pngSenlent_0-1657677006013.png

if no, you need to add these file to your project.

if yes,you may forget to add these file path,you can take a look at this post.

https://community.nxp.com/t5/S32K/S32K-S32DS-project-name-path-and-build-problem/td-p/1260029 

0 Kudos
Reply
2,303 Views
akhilranga
Contributor IV

Hello thee,

I didn't add them in my project. Hoping those files are available in NXP resources. May i know the process to add them in my project.

Thank You 

0 Kudos
Reply