Hi
I can't find the MWCD2D16S, and I'm not sure if the MWCD2D16S you're referring to is the MWCT2D16S.
In the S32K3 MCUs, there is not a power up/down sequence but the customer must respect the power-on ramp rate and the VREFH should always be equal to or less than VDD_HV_A +0.1.
Section 2.10.1 MCU Power Supply Ramp Rate in S32K3xx - Hardware Design Guidelines -- Rev_E2.pdf mentions the ramp rate of VDD_HV_A, VDD_HV_B and V15:

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------