MCTPTX1AK324 Code example build error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MCTPTX1AK324 Code example build error

跳至解决方案
4,078 次查看
Simone9
Contributor III

Good evening,

We have purchased the MCTPTX1AK324 demoboard for the development of PMSM motor control.
As a first test, we wanted to load the example code supplied with the demoboard: "S32K324 Triple PMSM Control Referece Design Development Board".

However, we encountered the compilation problem shown in the attached image.
How can this be solved?

The version of the IDE is S32DS v3.5.
The RTD pack is: S32K3 RTD AUTOSAR 4.4 Version 3.0.0.
The development package is the: S32K3xx development package version 3.5.0

Thanks for the support

0 项奖励
回复
1 解答
3,932 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@Simone9

please double-check if RTD 2.0.0 is already right installed.

below is mine, as you can see these demo in IDE

Senlent_1-1701224100186.png

and open "MCTPTX1AK324_Triple_PMSM_RDB_M7_0.mex"

Senlent_0-1701223974656.png

 

在原帖中查看解决方案

5 回复数
4,046 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@Simone9

this demo run's on RTD 2.0.0 + IPCF 3.6.0

please follow the step of the link below.

https://www.nxp.com/design/development-boards/automotive-development-platforms/s32k-mcu-platforms/s3... 

Senlent_0-1699855631612.png

0 项奖励
回复
4,038 次查看
Simone9
Contributor III

Hi,

Thanks for the reply.

I have tried to follow the suggested steps but have no problems with the inclusion of the required packages.

In the IDE's view of available extensions and packages there are only versions from 3.0.0 upwards of RTD.
I downloaded the ZIP of RTD 2.0.0 and tried to include it but apparently it failed.
I downloaded and installed the EXE of RTD 2.0.0 but again the outcome did not change.

I wanted to know if there were any special steps.

Thanks for the support

0 项奖励
回复
4,027 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@Simone9

belowing is my install step, it works fine on my side.

Senlent_0-1700017511711.png

 

0 项奖励
回复
3,946 次查看
Simone9
Contributor III

Hello,

I finally managed to get the project compiled and uploaded to the demoboard without any errors.

However, I wanted to look at the mex file to understand the configurations set in the various peripherals, but it gives me the following error:

Simone9_0-1701167587838.png

 The IDE version is 3.5 updated 6.

Thanks for the suppor.

0 项奖励
回复
3,933 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@Simone9

please double-check if RTD 2.0.0 is already right installed.

below is mine, as you can see these demo in IDE

Senlent_1-1701224100186.png

and open "MCTPTX1AK324_Triple_PMSM_RDB_M7_0.mex"

Senlent_0-1701223974656.png