Logging Lin data using s32k144 and Tja1020 driver

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Logging Lin data using s32k144 and Tja1020 driver

跳至解决方案
2,389 次查看
vcuongnv91
Contributor II

Hello everyboby...

I am woking with a project using S32k144 and tja1020 lin driver. I can use the hardware as master or slave for simulating data on lin bus. My problem is i can find any way for logging Lin data on Lin buss, if there are both real master and slave nodes on bus.

With flexcan, we have Listen-only mode for this case, but as i know, there is no mode like this for Lin driver. So could any body have solution for this case? Thankyou very much at all...

标记 (1)
0 项奖励
回复
1 解答
2,279 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @vcuongnv91,

I think this is the best solution -using another UART module to monitor the RX line from the transceiver.

Regarding transceivers, there are some devices that have a Listen only modes, for example UJA113X, but this is not the issue here.

https://www.nxp.com/docs/en/data-sheet/UJA113X_SER.pdf

 

Regards,

Daniel

 

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,383 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @vcuongnv91,

The simplest and most effective solution would be to use a tool like the PEAK-System PLIN-USB. It allows for passive tracing of LIN bus communication without interfering with the signal, making it ideal for debugging and monitoring purposes.

 

BR, Daniel

2,351 次查看
vcuongnv91
Contributor II
At this time, my solution is using an other uart channel connect with LpUart-Lin channel for reading data after receiving Header from Lin bus. And it is working fine. Is there any solution better than this?
0 项奖励
回复
2,280 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @vcuongnv91,

I think this is the best solution -using another UART module to monitor the RX line from the transceiver.

Regarding transceivers, there are some devices that have a Listen only modes, for example UJA113X, but this is not the issue here.

https://www.nxp.com/docs/en/data-sheet/UJA113X_SER.pdf

 

Regards,

Daniel

 

0 项奖励
回复
2,359 次查看
vcuongnv91
Contributor II
Thankyou very much for your quickly reply. With s32k1 / s32k3 and Lin driver like TJA1021 / TJA1124 / SJA1124, is there any solution for logging Lin data like PLin-USB of KEAK-System? Or we must select other hardware for this?
0 项奖励
回复