Logging Lin data using s32k144 and Tja1020 driver

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Logging Lin data using s32k144 and Tja1020 driver

ソリューションへジャンプ
2,394件の閲覧回数
vcuongnv91
Contributor II

Hello everyboby...

I am woking with a project using S32k144 and tja1020 lin driver. I can use the hardware as master or slave for simulating data on lin bus. My problem is i can find any way for logging Lin data on Lin buss, if there are both real master and slave nodes on bus.

With flexcan, we have Listen-only mode for this case, but as i know, there is no mode like this for Lin driver. So could any body have solution for this case? Thankyou very much at all...

タグ(1)
0 件の賞賛
返信
1 解決策
2,284件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @vcuongnv91,

I think this is the best solution -using another UART module to monitor the RX line from the transceiver.

Regarding transceivers, there are some devices that have a Listen only modes, for example UJA113X, but this is not the issue here.

https://www.nxp.com/docs/en/data-sheet/UJA113X_SER.pdf

 

Regards,

Daniel

 

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,388件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @vcuongnv91,

The simplest and most effective solution would be to use a tool like the PEAK-System PLIN-USB. It allows for passive tracing of LIN bus communication without interfering with the signal, making it ideal for debugging and monitoring purposes.

 

BR, Daniel

2,356件の閲覧回数
vcuongnv91
Contributor II
At this time, my solution is using an other uart channel connect with LpUart-Lin channel for reading data after receiving Header from Lin bus. And it is working fine. Is there any solution better than this?
0 件の賞賛
返信
2,285件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @vcuongnv91,

I think this is the best solution -using another UART module to monitor the RX line from the transceiver.

Regarding transceivers, there are some devices that have a Listen only modes, for example UJA113X, but this is not the issue here.

https://www.nxp.com/docs/en/data-sheet/UJA113X_SER.pdf

 

Regards,

Daniel

 

0 件の賞賛
返信
2,364件の閲覧回数
vcuongnv91
Contributor II
Thankyou very much for your quickly reply. With s32k1 / s32k3 and Lin driver like TJA1021 / TJA1124 / SJA1124, is there any solution for logging Lin data like PLin-USB of KEAK-System? Or we must select other hardware for this?
0 件の賞賛
返信