Lisence missing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Lisence missing

9,432件の閲覧回数
jiangjian
Contributor II

Dear :

我的S32DS安装使用20天左右,出现“Lisence missing”,进行offline request,点击Active进行保存,出现错误对话框“Software Activation Code error”,对话框正文信息如下:

CLLReason [errorNo=16,errorString=Error creating activation handle.(FNP error 50003,71000,10104),flxActMajorErrorNo=50003,flxActMinorErrorNo=71000,flxActSysErrorNo=10104,flxCommErrorNo=0]

请协助解决,此问题如何处理,谢谢!

0 件の賞賛
返信
7 返答(返信)

9,427件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

If you reenter activation code it is still not working?

Which version of S32DS are you trying to activate? I can see you have 2 versions in our system.

Best regards,

Peter

0 件の賞賛
返信

9,275件の閲覧回数
Lingya
Contributor I
Hello petervlna: Sorry to bother you. I am confused by the same problem for few days. Product:S32 Design Studio fot PA 2017.R1, Version:2.0,Status:License missing; License key:S32 Design Studio for e200 v2.0 when I try to activate S32, it showed “CLLReason [errorNo=16,errorString=Error creating activation handle.(FNP error 50003,71000,10104),flxActMajorErrorNo=50003,flxActMinorErrorNo=71000,flxActSysErrorNo=10104,flxCommErrorNo=0]” I tried to reset “flexnet licensing service” but it didn't work. Could you help me to deal with it? Thank you in advance.
0 件の賞賛
返信

9,243件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Under what email is the license registered?

I can check in our system where is the issue.

Best regards,

Peter

0 件の賞賛
返信

9,404件の閲覧回数
jiangjian
Contributor II

HELLO:

这个问题目前已处理好了。

原因是近期安装其他软件(xShell7)存在无反应问题,为了处理这个问题将PC服务里边把flexnet licensing service服务停止掉,并把启动类型改成禁止后导致S32DS Lisence missing问题产生。

目前将此服务恢复后,S32DS Lisence missing问题已不存在了。

感谢NXP技术百忙中的支持!

 

7,590件の閲覧回数
shiweili
Contributor I
牛逼!
0 件の賞賛
返信

9,193件の閲覧回数
LIHAN_FLYING
Contributor II

it's works

0 件の賞賛
返信

9,168件の閲覧回数
jiangjian
Contributor II

It's already working

0 件の賞賛
返信