Lin interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Lin interface

7,431件の閲覧回数
123456789Raji_20
Contributor I

hi ,

myself Rajeshwari present am working on S32K344 version 3.4  i taken Example code from Nxp website  :name is LIN Lin_Ip_FrameTransfer_S32K344 i want flash this code on Battery management System kit when am flashing this code am unable to get output can u help in this to solve this problem .

 

Thanks and Regards,

Rajeshwari 

0 件の賞賛
返信
9 返答(返信)

7,424件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

if you meant RD-K344BMU board, then there is no LIN transceiver on it and pins used in the example are used for other purposes. You can check board schematic and try to find some free pins with LPUART functions, like uart_tx/uart_rx lines, and connect external LIN transceiver if needed.

BR, Petr

0 件の賞賛
返信

7,402件の閲覧回数
123456789Raji_20
Contributor I
actually in NXP Board S32K344 -Q172 im checking LIN output at pin number 7 and 8 (Jumper 23 )
0 件の賞賛
返信

7,414件の閲覧回数
123456789Raji_20
Contributor I

I checked BMU board PTB27,28,9,10 pin are using for LIN interface im using logic analyzer and logic analyzer software tool for display...................i downloaded already LIN stack S32K344 RTD 0.9.0 with this i cant see the output (tx data and rx data  

0 件の賞賛
返信

7,412件の閲覧回数
123456789Raji_20
Contributor I

then for that example code how i have to check tx and rx data can u please explian me 

0 件の賞賛
返信

7,408件の閲覧回数
123456789Raji_20
Contributor I
I checked BMU board PTB27,28,9,10 pin are using for LIN interface im using logic analyzer and logic analyzer software tool for display...................i downloaded already LIN stack S32K344 RTD 0.9.0 with this i cant see the output (tx data and rx data
0 件の賞賛
返信

7,369件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

can you share (or point to) board schematic you have? At what board's location are you connecting with analyzer.

BR, Petr

0 件の賞賛
返信

7,364件の閲覧回数
123456789Raji_20
Contributor I

This schematic diagram im using present no NXP-S32K344-Q172 board im seeing output at j23 pin number 8 and 7 

0 件の賞賛
返信

7,356件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

LIN Lin_Ip_FrameTransfer_S32K344 is a simple demo example which shows a communication between a Lin Master and a Lin Slave of both Lpuart Ip and Flexio Ip. As example does communication between LIN Master/Slave on the board  you should connect J23.7 to J23.8 and place either J20 or J24 jumper. Then 2 LIN frames should be visible on this LIN bus connection after example running. You can use scope or analyzer to see LIN frames. This is what you should get
Image_2023-06-06_10-04-02.pngImage_2023-06-06_10-04-02.png

BR, Petr

0 件の賞賛
返信

7,278件の閲覧回数
123456789Raji_20
Contributor I
i connected jumper connection where i have to check my output in jumper 23 (7 & and 8 pin by using logic analyzer. Now present from jumper 23 7 and 8 pin i shorted i taken one more connection i gave to logic analyzer am not getting output i shorted jumper 20 also
0 件の賞賛
返信