Lin diagnostics code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Lin diagnostics code

2,869 Views
pankajprasad100
Contributor III

Hi,

I am working on S32K116 MCU and s32 design studios IDE, i need to implement LIN DIAGNOSTICS using lin apis.

 

If some one provide example code how to use these apis, that's really helpful for us.

 

Diagnostic request ID-3c

For example i need to send 

7E 02 10 03 00 00 00 00

 

 

Thanks & Regards

PANKAJ PRASAD

0 Kudos
Reply
4 Replies

2,850 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

try to refer to "lin_master_baremetal_s32k116" demo example within S32 design Studio.
With this code you can send any frame to need.

Br, Petr

0 Kudos
Reply

2,832 Views
pankajprasad100
Contributor III

Hi,

 

   I need to use apis in lin_diagnostics_services.c to implement the code.

 

Location:

         SDK>middleware>lin>lin_diagnostics_services.c

 

 

Thanks & Regards

Pankaj prasad.

0 Kudos
Reply

2,823 Views
PetrS
NXP TechSupport
NXP TechSupport
0 Kudos
Reply

2,811 Views
pankajprasad100
Contributor III

Thank you for the information...

0 Kudos
Reply