Jflash(V6.84b) cannot erase the S32K146 chip,Failed to blank checking...

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Jflash(V6.84b) cannot erase the S32K146 chip,Failed to blank checking...

1,257 Views
Leon-Jiang
Contributor I

Chip:S32K146

Tool:Jlink V9

Question: Use Jflash(V6.84b) to connect to S32K146, but can not execute the erase flash instruction.

 

Detailed steps are as follows:

 

STEP1: connect to S32K146,the message "Connection successful" is displayed.

1.png

STEP2:  Select Target -> Manual Programming -> Erase Chip

2.png

STEP3: Error message:Failed to blank checking...

3.png

 

I would like to ask how to solve the above problems, the chip a few days ago is still good, today is not brush program.

 

 

 

0 Kudos
Reply
1 Reply

1,234 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@Leon-Jiang

      Your programming operation is not standardized, many necessary inspection steps are ignored, you can refer to this article, and there are some registers to see what causes the possible causes of the programming failure.

       https://mp.weixin.qq.com/s?__biz=MzI0MDk0ODcxMw==&mid=2247485716&idx=1&sn=979631aa2385a4e3c7651ee75e... 

This is the solution to a similar problem ,

https://community.nxp.com/t5/S32K/Unbricking-S32K146/m-p/937227 

BR!

    Jim.

0 Kudos
Reply