Launching MCSPTEAK116_BLDC_6Step_Debug Failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Launching MCSPTEAK116_BLDC_6Step_Debug Failed

1,691 Views
Chen2002
Contributor I

I am trying to run the MCSPTEAK116_BLDC_6Step example on the S32K116 EVK and MOTOR-GD daughterboard. I was able to build the code but fail to debug. However, I can compile and debug when I use the software's routines, such as Hellow World. 

Chen2002_0-1707205862378.png

My configuration is shown below.

Chen2002_1-1707205974294.png

I tried the method described in the link ,but it didn't work.

Internal error during Start GDB Semihosting Job on... - NXP Community

What should I do to solve this question? Thank you very much!

 

 

 

0 Kudos
Reply
3 Replies

1,663 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @Chen2002 

could you share the project, so I can test it on my side? Which S32DS version is used?

Regards,

Lukas

0 Kudos
Reply

1,658 Views
Chen2002
Contributor I

Thanks for your reply!

The software I use is S32 Design Studio for ARM Version 2.2. And I downloaded the Development Kit - Application Software according to Get Started with the MCSPTE1AK116.

I followed this tutorial step by step, but unfortunately I didn't suceed. I wonder if there is something incompatible with the project(MCSPTE1AK116_BLDC_6Step), because it was released in 2022.

Thank you!

Chen

 

0 Kudos
Reply

1,644 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Well, your project works on my side. I also tried to create own project from the original MCSPTEAK116_BLDC_6Step project and it's working too.

It seems to be a problem with the debugger. Please take a look at following threads, it could help:

https://community.nxp.com/t5/S32K/Internal-error-during-Start-GDB-Semihosting-Job-on-S32DS/td-p/1730...

https://community.nxp.com/t5/S32K/Unable-to-Debug-project-using-PEMicro-Debugger/td-p/1730488

Regards,

Lukas

0 Kudos
Reply