LPi2c Driver - FreeRTOS issue : I could not generate multiple i2c data

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPi2c Driver - FreeRTOS issue : I could not generate multiple i2c data

1,321件の閲覧回数
well29
Contributor I

I followed the recommendation to successfully fix issue of lpi2c and freertos integration from
S32K142: lpi2c is not working with freeRTOS integration. - NXP Community.

The problem is that when I use LPI2C_DRV_MasterSendDataBlocking function to write data with big size like in example foo function below, it could not write the whole data block and would send stop after around 4 bytes. The same function works without FreeRtos but not with it. 

foo(uint8_t reg, uint8_t* data, uint16_t count) {
uint8_t dt[256];
dt[0] = reg;
uint8_t i;
for(i = 0; i < count; i++)
dt[i+1] = data[i];

LPI2C_DRV_MasterSendDataBlocking(INST_LPI2C0, dt, count+1, true, 10);

}

I'm using S32 Design Studio for S32 Platform Version: 3.5 Build id: 220726. 
I used the freeRtos example and added i2c peripheral.

Is there a way to quickly solve this?

0 件の賞賛
返信
3 返答(返信)

1,254件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @well29,

Is the driver initialized inside a FreeRTOS task after the scheduler is started?

 

Thank you

 

0 件の賞賛
返信

1,228件の閲覧回数
well29
Contributor I

Yes, the i2c works. It's just that it's capped to about 5-10 sent data bytes. I'm trying to send about 128 data bytes and that's where it failed.

0 件の賞賛
返信

1,222件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @well29,

Does the function return, what is the status?

Have you tried the non-blocking function?

 

Thank you

0 件の賞賛
返信