LPSPI multi master configuration example

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPSPI multi master configuration example

Jump to solution
9,770 Views
Saitej
Contributor IV

Hi 

Here am with S32K 148 EVB & here am with 6 sensors(slaves) that need to communicate over SPI channel, As I see S32K will support only 4 chip selects, how to achieve communication with 6 sensors ? (am using SPI PAL drivers from processor expert configuration).S32K 148 is the master.

Also can some one provide me the example on LPSPI multi master configuration on same SPI channel (SPI0).

Thank you in advance ! 

 

0 Kudos
Reply
1 Solution
9,713 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello,

Which SDK version do you use?

The LPSPI_DRV_SetPcs() function takes 3 parameters including PCS polarity.

Please step the function and double-check if the TCR command (which_pcs, polarity) is correct.

 

Thanks,

BR, Daniel

View solution in original post

0 Kudos
Reply
5 Replies
9,743 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

The LPSPI0 module supports only 4 PCS.

But the S32K148 MCU has 6 LPSPI0 PCS pins.

danielmartynek_0-1607514529957.pngdanielmartynek_0-1607514529957.png

So you could use all of the PCS pins.

For example LPSPI0 PCS0 can be either PTA26 or PTB0.

The port module would need to be reconfigured so that the LPSPI0 module can control the correct pin before a transfer is triggered.

We don't have such an example though.

 

Regards,

Daniel

 

0 Kudos
Reply
9,718 Views
Saitej
Contributor IV

Thankyou for the response 

But re initialising the port pins at the run time may cost the time.

Capture.JPGCapture.JPG

Here I have attached my code , in which SPI0 is the master and SPI1 and SPI2 are the slaves , if am communicating alone with SPI1 or SPI2 it is working fine able to send & receive data properly. but if SPI1 and SPI2 sharing the SDI & SDO, SCLK lines of SPI0 then am seeing master received data is "255".

uint8_t master_send[BUFFER_SIZE] = {1, 2, 3, 4, 5, 6, 7, 8, 9, 10};
uint8_t master_receive[BUFFER_SIZE];
uint8_t slave_send[BUFFER_SIZE] = {1, 2, 3, 4, 5, 6, 7, 8, 9, 10};
uint8_t slave_receive[BUFFER_SIZE];
volatile uint8_t i = 0;
uint8_t frame_sent = 1;
volatile uint32_t swt = 0;

CLOCK_SYS_Init(g_clockManConfigsArr, CLOCK_MANAGER_CONFIG_CNT,g_clockManCallbacksArr, CLOCK_MANAGER_CALLBACK_CNT);
CLOCK_SYS_UpdateConfiguration(0U, CLOCK_MANAGER_POLICY_AGREEMENT);

PINS_DRV_Init(NUM_OF_CONFIGURED_PINS, g_pin_mux_InitConfigArr);
PINS_DRV_ClearPins(GPIO_LED, RED_LED);
/* Initialize SPI0 */
SPI_MasterInit(&spi1Instance, &spi1_MasterConfig0);
//SPI_MasterInit(&spi1Instance, &spi1_MasterConfig1);
/* Initialize SPI1 */
SPI_SlaveInit(&spi2Instance, &spi2_SlaveConfig0);
//SPI_SlaveInit(&spi3Instance, &spi3_SlaveConfig0);

PINS_DRV_SetPins(GPIO_LED, GREEN_LED);
OSIF_TimeDelay(500);
PINS_DRV_ClearPins(GPIO_LED, GREEN_LED);

while(1)
{

SPI_SlaveTransfer(&spi2Instance, slave_send, slave_receive, NUMBER_OF_FRAMES);
SPI_MasterTransferBlocking(&spi1Instance, master_send, master_receive, (uint8_t) NUMBER_OF_FRAMES, (uint8_t) TIMEOUT);
/* verify that the data received is correct */
frame_sent = 1;
for(i = 0U; i < BUFFER_SIZE; i++)
{
if((slave_send[i] != master_receive[i]) || (master_send[i] != slave_receive[i]))
{
frame_sent = 0;
break;
}
}
if(frame_sent == 0)
{
//PINS_DRV_SetPins(GPIO_LED, BLUE_LED);
PINS_DRV_ClearPins(GPIO_LED, BLUE_LED);
}
else
{
PINS_DRV_SetPins(GPIO_LED, BLUE_LED);
//PINS_DRV_ClearPins(GPIO_LED, BLUE_LED);
}

SPI_SetSS(&spi1Instance, spi1_MasterConfig1.ssPin);
SPI_SlaveTransfer(&spi3Instance, slave_send, slave_receive, NUMBER_OF_FRAMES);
SPI_MasterTransferBlocking(&spi1Instance, master_send, master_receive, (uint8_t) NUMBER_OF_FRAMES, (uint8_t) TIMEOUT);
/* verify that the data received is correct */
frame_sent = 1;
for(i = 0U; i < BUFFER_SIZE; i++)
{
if((slave_send[i] != master_receive[i]) || (master_send[i] != slave_receive[i]))
{
frame_sent = 0;
break;
}
}
if(frame_sent == 0)
{
PINS_DRV_SetPins(GPIO_LED, RED_LED);
//PINS_DRV_ClearPins(GPIO_LED, RED_LED);
}
else
{
//PINS_DRV_SetPins(GPIO_LED, RED_LED);
PINS_DRV_ClearPins(GPIO_LED, RED_LED);
}
}

Small observation here all the time am seeing Slave side CS pin (SPI1) is high even after SPI transaction.

attached processor expert configuration screen shots

Thanks in advance

0 Kudos
Reply
9,714 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello,

Which SDK version do you use?

The LPSPI_DRV_SetPcs() function takes 3 parameters including PCS polarity.

Please step the function and double-check if the TCR command (which_pcs, polarity) is correct.

 

Thanks,

BR, Daniel

0 Kudos
Reply
9,690 Views
Saitej
Contributor IV

Hello,

am using S32K148_SDK 3.0.0

Yes, in debug mode cross verified the TCS register it is updating as per requirement. Even in the logic analyser we can see CS is working as expected & even MOSI line also working as expected.

But MISO is line is continuously high.

SPI1.JPGSPI1.JPGSPI1_2.JPGSPI1_2.JPG

 

0 Kudos
Reply
9,683 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello,

It seems like the slave modules do not detect the PCS.

All I see from the attachments is that the slave modules are routed to 2 PCS each in PORT.

But are the slave modules configured to the correct PCS in LPSPI?

Also, get the status of the slave transfers with LPSPI_DRV_SlaveGetTransferStatus().

 

Thanks,

BR, Daniel

0 Kudos
Reply