LPSPI Voltage Levels

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPSPI Voltage Levels

1,392 Views
Pouya
Contributor II

Hi,

I am having trouble interfacing S32K344 LPSPI with TMS570 mibSPI. What is the VIH, VOH, VIL, and VOL for S32K344 LPSPI SCK, CS, SOUT, and SIN pins?

Thanks,

Pouya 

0 Kudos
Reply
1 Reply

1,385 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

It is given by use power supply rail and its configuration (5V or 3.3V). LPSPI pads can be on both supply levels, either VDD_HV_A or VDD_HV_B (pay attention to excel sheet S32K344_IOMUX.xlsx, embedded in the device’s RM).

VIH/VIL you will find defined in DS, Table 22 and 23.

VOH/VOL I have found it only indirectly stated within IOH and IOL specification as condition for this current measurement.

For instance for IOH_33 condition is VOH >= VDD_HV_A/B - 0.7V

It means V-I characteristic of the pin can be estimated by linear approximation between points and < IOH_33; VDD_HV_A/B - 0.7V> and <0mA ; VDD_HV_A/B>.

The same way IOL_33 condition is VOL <= 0.7V.

It implies V-I characteristic as < IOL_33 ; 0.7V > and < 0mA ; 0V >

However it is expected that SPI output lines and connected to high impedance input, so you can just simplify it to expect VOH = VDD_HV_A/B and VOL = VSS (i.e. 0V).

0 Kudos
Reply