LPSPI SEND question.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPSPI SEND question.

Jump to solution
1,308 Views
mswd
Contributor I

hi.

i would like to use the send function of LPSPI0.

(LPSPI_DRV_MasterTransferBlocking)

but now there is no signal.(oscilloscope)

 

Attachment 1. H/W circuit diagram.

Attachment 2. config setting.

Attachment 3. code init.

 

i have a question here.

Is transmisson possible even with only LPSPI0_OUT?

Or should I connect another pin? (ex. LPSPI0_PCS1)

 

only the send function is needed.

what are the requirements for that feature?

 

(i using 32K146)

 

thank you.

0 Kudos
Reply
1 Solution
1,287 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

As the Master, you should at least initialize the Serial Clock pin.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,288 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

As the Master, you should at least initialize the Serial Clock pin.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply