LIN Stack CRC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LIN Stack CRC

1,979件の閲覧回数
nxp_user001123
Contributor III

Hi,

Just a quick question. Based on the LIN stack example, we imported another LDF-File (Version 2.1) generated everything., compiled, flashed. Microcontroller is sending, but on our PC-program for simulating the LIN-Slave we had to change the CRC from enhanced (LIN 2.0) to classic CRC (LIN 1.3). So that communication in both directions is working.

We expected : LIN enhanced CRC (because LDF-File is Version 2.1) from NXP microcontroller.

So can we change the used CRC in the NXP S32DS linstack module?

 

Thanks in advance!

タグ(2)
0 件の賞賛
返信
3 返答(返信)

1,934件の閲覧回数
nxp_user001123
Contributor III

Hi Daniel,

Yes sure:

RTD : 5_0

LIN Stack : 2_0_5

 

We are using the eval board  S32K3X4EVB-T172

 

0 件の賞賛
返信

1,920件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @nxp_user001123,

Can you share the LDF?

What frame types do you send?

danielmartynek_0-1734514643365.pngdanielmartynek_0-1734514643365.png

 

0 件の賞賛
返信

1,951件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @nxp_user001123,

Can you please specify the S32K part number, SDK/RTD version and the LIN Stack version?

 

Thank you,

BR, Daniel

0 件の賞賛
返信