LIN Stack CRC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LIN Stack CRC

2,114 Views
nxp_user001123
Contributor III

Hi,

Just a quick question. Based on the LIN stack example, we imported another LDF-File (Version 2.1) generated everything., compiled, flashed. Microcontroller is sending, but on our PC-program for simulating the LIN-Slave we had to change the CRC from enhanced (LIN 2.0) to classic CRC (LIN 1.3). So that communication in both directions is working.

We expected : LIN enhanced CRC (because LDF-File is Version 2.1) from NXP microcontroller.

So can we change the used CRC in the NXP S32DS linstack module?

 

Thanks in advance!

Tags (2)
0 Kudos
Reply
3 Replies

2,069 Views
nxp_user001123
Contributor III

Hi Daniel,

Yes sure:

RTD : 5_0

LIN Stack : 2_0_5

 

We are using the eval board  S32K3X4EVB-T172

 

0 Kudos
Reply

2,055 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @nxp_user001123,

Can you share the LDF?

What frame types do you send?

danielmartynek_0-1734514643365.png

 

0 Kudos
Reply

2,086 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @nxp_user001123,

Can you please specify the S32K part number, SDK/RTD version and the LIN Stack version?

 

Thank you,

BR, Daniel

0 Kudos
Reply