K396 EVB example error troubleshoot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

K396 EVB example error troubleshoot

3,596 次查看
Harry0001
Contributor II

Now i tested the demo example project of the S32 k396,and i found that after changing the pin and updating the generation code,then compliing it ,it shows the following error:

workspaceS32DS.3.5/Lighting_SingleCore_S32K396_M7/Lighting_SingleCore_S32K396_M7/swc/rte/generic/include/SwcRte.h:39:10: fatal error: SwcRte_Cfg.h: No such file or directory

SwcRte_Cfg.h file can be found out in the porject  before i updating the generation code,i want to know why it miss after i clicking the update button of the S32 v3.5?What should i do to solve this error?

0 项奖励
回复
4 回复数

3,588 次查看
Harry0001
Contributor II

it seems that before it is called "SwcRte_Cfg",after updating it change to "SwcRte_PBcfg"!Should i rename it name to "SwcRte_cfg"?

0 项奖励
回复

3,557 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,

That is because your project is generated as post build (PBcfg) instead of precompile (CFG).

Those are 2 basic AUTOSAR structures for project generation.

Please select the precompile one in order to get CFG files linked.

For more details please refer to basic autosar trainings.

Best regards,

Peter

0 项奖励
回复

3,542 次查看
Harry0001
Contributor II

“Please select the precompile one in order to get CFG files linked.

Please tell me where to chose the precompile setting,i am confused for that.

Other question is that i cannot find the file for S32 opening but only finding the example file for EB,as is the attached picture showing,i have downloaded the updated software package which updated time is April,2023 ,what is the point of this problem?Thanks!

0 项奖励
回复

3,525 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Please tell me where to chose the precompile setting,i am confused for that

You can select it in your configuration tool. For example:

petervlna_0-1691736545645.png

Other question is that i cannot find the file for S32 opening but only finding the example file for EB

Well hard to say. I could be that there are no S32DS examples. But the sample SW is usually provided directly in plugins:

petervlna_1-1691737166952.png

Best regards,

Peter

 

0 项奖励
回复